Back to top

AB Micrologix PLC to AKD Basic over Modbus

This sample has three parts.  one is the PLC code, one is the drive parameters and one is the BASIC program to run in the drive.  I use dynamic mapping to read a number of drive parameters with one MSG block.  I created BASIC variables and read them with just one MSG block.  I also have an enable and disable message.