Back to top

AKD DC Bus Link

This article is a single-source data for AKD content.

  • Brake circuit: with dynamic distribution of the regenerated power between several amplifiers on the same DC bus link circuit.
  • Internal Brake Resistor standard in most types, external Brake Resistor if required.
  • DC bus link voltage can be connected in parallel
  • Only servo amplifiers with mains supply from the same mains (identical mains supply voltage) may be connected by the DC bus link
  • KCM Capacitor Module for AKD with 400/480V rated voltage and max. 24A rated current.