Back to top

AKD Ethernet IP Diagnostics and Dynamic Mapping

Application Note on AKD Etherent IP Diagnostics and Dynamic Mapping when used with Contrologix or Compactlogix PLCs.

Comments

toddevans01's picture
toddevans01
Note at the time of Workbench and FW 1-15, when dynamically mapping instances using the Workbench GUI, if the Ethernet IP screen in the project tree was exited and re-entered, Workbench would reorder the instances in numerical order rather than keeping the order used when the Configure was used.
This was reported and an update with fix will occur in Workbench 1-16 soon to be released.
Just be aware this can happen.