Back to top

AKD MOTOR.BRAKE setting for low current brakes

In some application low current brakes are used which may cause the drive to fault on F305 Brake Open Circuit.
Cause:
Motor brake open circuit. Fault threshold is 200 mA.
Remedy:
Check cabling and general functionality.

For special low current brake applications, the F305 fault can be bypassed

using the setting MOTOR.BRAKE = 100 set via the Workbench terminal.

Once set, the brake state on the brake screen will show: 100-brake is fitted-fault ignored.