Back to top

KAS PxMM Controller Connected to a Control Logix PLC Through EtherNet/IP

This article is divided up into the following:

  • Application note
  • PDMM project
  • Rockwell project
  • PDMM EDS file(s)

This application note has two parts. Chapter 1 is an in-depth, step-by-step “how to” of adding Ethernet/IP communications to a KAS project as well as adding KAS support to a new or existing RSLogix5000 project. Chapter 2 is a hands-on quick start guide that explains how to upload the KAS EIP sample projects (.kas & .ACD files) in order to demonstrate correct setup / working Ethernet/IP communications.