Back to top

Decentralized Drive System

The AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives.

image
 

Blue Boxes: All components in the blue box are products delivered by Kollmorgen. For detailed information click to the product or use the table below for navigation.
Gray Boxes: Elements in the gray area are components which have to be added by the machine builder.

AKD-C AKD-C Power Supply
AKD-N AKD-N Drive
AKD-CN-Coupling Connector interface for cabinet wall (in process)
AKD-M AKD PDMM Drive
AKC Touchscreen IPC
AKM AKM Motor
AKMH AKMH Motor
AKI Operating Console
AKT KAS Input and Output Terminals
BAR/BAS/BAFP Brake Resistor
Cx Cables Configured CC/CM/CF cables for connection of the components, refer to the cable part number scheme
DDL Linear motors (on request)
ENCP Ethernet cables
Gearhead Micron Gearheads
Heatsink Kit optional accessory for AKD-N
KAS-IDE KAS System Setup Tool
KBM KBM Motor
KCM KCM Capacitor Module
Redi Mount Adapters to mount Micron Gearheads to AKM motors
Workbench AKD Setup Tool