Back to top

DRIVE-CLiQ

DRIVE-CLiQ is an open encoder interface. Kollmorgen offers AKM Motors with singleturn or multiturn Encoders and DRIVE-CLiQ Interface. The Motor feedback can be connected via an M12 connector to the SINAMICS drive System.

Temperature sensor type in the Motor is selected according to the current Siemens requirements.

Comments

Jonatas's picture
Jonatas
Hello Will and all,
We are offering our AKMH solution to a big OEM in Brazil which uses Sinamics S120 Drives. They want to keep their Servodrive standard unchanged and test our AKMH solution with that.
What Encoder type could we use to make the solution compatible ?
Tks in advance.
Will Gaffga's picture
Will Gaffga
Hi Jonatas,
I'll make sure this gets passed on to the best person to answer your question.
Thanks!