Back to top

EtherNet IP Bus

EtherNet/IP (EtherNet Industrial Protocol) is an Ethernet-based fieldbus which is primarily used in the field of automation technology. The bus was developed by Allen-Bradley and later transferred to the ODVA organization as an open standard. EtherNet/IP was then published as an open industry standard in the year 2000.

The typical cycle time of an EtherNet/IP network is 10ms, which means that the system is capable of meeting real-time software requirements for industrial I/Os. For tough real-time requirements, for example in servo drives, protocol extensions are available that reduce the jitter for controlling servomotors to values in the sub-microsecond range using precise time synchronization in line with IEEE1588.

Comments

Kevin's picture
Kevin
Are there communication issues with older versions of Allen Bradley controllers, using RSLogix Version 17 for example?