Back to top

How to Configure A BiSS C Rotary Encoder with an AKD

The AKD makes the setup more convenient for the user by not requiring them to convert the BiSS encoder’s bit resolution.  When using a rotary Renishaw BiSS C encoder the parameter FB1.ENCRES always requires the value 4294967295, which is (2^32) – 1.  The parameter BISSBIT does have to configured by the user to the bit resolution of the BISS encoder.

 

 

I

 

Comments

Peter Yoon's picture
Peter Yoon
In case the parameter FB1.BISSBITS is 26, Not 32, What is the FB1.ENCRESS value?
Is it same to (2^32) - 1? or (2^26) -1?
kenny.hampton@kollmorgen.com's picture
kenny.hampton@k...
Hello Peter

When using a rotary BiSS C encoder the parameter FB1.ENCRES always requires the value 4294967295, which is (2^32) – 1.