Back to top

KAS Interface App Using HTTP Request Programmed in Android Studio

The KASIface application is to show how a KAS-variable access can be implemented into a mobile device. This example uses http request in the text format. The programming is done with Java in Android Studio.

 image

The download portion contains:

  • Signed APK, ready to install on a Andorid device
  • AsyncTask function, to be used for read or write of any KAS variable
  • Java Main, containing the full code used for the app
  • XML, containing the screen setting for the app
  • Manuals on how to use this example and code snippets

More information can be found with the following links.

http://kdn.kollmorgen.com/webhelp/kas/#AdvancedTopics/ReadWritePLCVars/ReadWritePLCVars.htm

http://kdn.kollmorgen.com/webhelp/kas/#AdvancedTopics/HTTP_basic.htm

http://kdn.kollmorgen.com/content/kas-interface-using-http-request-programmed-vb2008

http://kdn.kollmorgen.com/content/kas-http-communication

Attachment: