Back to top

Loading and saving application parameters (recipes) to NVRAM memory.

The attached KAS project adds a program (LoadSaveParams) to one of the standard 2 axis startup templates to store

and retrieve parameter settings from the PDMM’s NVRAM memory.An Array of Structures with the following elements

was setup:

MotorParameter[x].Position

MotorParameter[x].Velocity

MotorParameter[x].Acceleration

MotorParameter[x].Deceleration

 

 

A Control Panel was added to the project to enter values and perform the save or to retrieve values already save.