Back to top

Old Smartdrive

0 votes
+ vote
Vote up!

Hi!! 

I am working whit a old drive: SmartDrive. I installed MotionLink for SmartDrive but I need a TL file to configure motor parameters. 

The motor is a GOLDLINE BRUSHLESS; model: B-106-A-31-R3. 

Could you send me the file, or give me information about where I can download. 

Thanks!! 

Comments

Thanks for your replay!
I have the model D03001 of the SmartDrive, I have a doubt regarding the connection of the DC Bus + and the DC Bus -.

What do I have to connect to these terminals?

Daniel Barradas - Mon, 10/30/2017 - 14:33
Log in or register to post comments

2 Answers

1 vote
+ vote
Vote up!

The motor's  parameter file can be loaded from the Smart Drive Software "GUI".  You are required to select the B-106-A motor in the GUI software.

This is a link to Smart Drive Software:

http://www.kollmorgen.com/en-us/products/drives/discontinued/discontinued-drives/

Scroll down to the header Smart Drive (KOL) and the software file is listed as  (Smart Drive Software Rev.1)

0 Comments

0 votes
+ vote
Vote up!

Attached is the Catalog Data Sheet containing the motor parameters.

These motor parameters may be entered into the SmartDrive via the MotionLink software.

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.