Back to top

PDMM - Coordinated Motion Example with Ethernet/IP Interface to a Vision System

The attachments outline a KAS Application with the following features:

  • 3 axis coordinated motion
  • Banner vision camera connected to the PDMM via Ethernet/IP
  • Camera reads a barcode and  sends the information through Ethernet/IP to the PDMM.
  • The bar code value is then used to determine which pattern to run