Back to top

Setup Software

General

The servo amplifiers must be adapted to the requirements of your machine. Usually you will not have to carry out this parameter setting yourself on the amplifier, but on a PC, with the assistance of the setup software. The PC is connected to the servo amplifier by a null-modem cable (serial). The setup software provides the communication between the PC and the servo amplifier.

Workbench for AKD

workbench.jpg

Workbench will run under WINDOWS 2000 / XP / Vista and WINDOWS 7. The functioning of the software has not been tested for WINDOWS running within Unix or Linux.

The latest version of the setup software can be downloaded from the Downloads page or from our website.

DriveGUI for S300/S700

drivegui_en.jpg

DriveGUI.exe will run under WINDOWS 2000 / XP / Vista and WINDOWS 7. The functioning of the software has not been tested for WINDOWS running within Unix or Linux.

The latest version of the setup software can be downloaded from the Downloads page or our website.

The Online Help S300 S700 integrated in the software (incl. ASCII Object Reference) can be started independently.

SafetyGUI for Safety cards S1-2/S2-2

safetygui_en.jpg

DriveGUI.exe will run under WINDOWS 2000 / XP / Vista and WINDOWS 7.

The latest version of the setup software can be downloaded from the Downloads page or our website.

The errors messages are described in file Error Codes.

Drive for S400 / S600

drive_en.jpg

Drive.exe will run under WINDOWS 95c / 98 / 2000 / ME / XP and WINDOWS NT 4.0. The help system cannot be used with Windows 95a and 95b. Drive.exe will not work with WINDOWS 3.xx, DOS and OS2.

The latest version of the setup software can be downloaded from the Downloads page or our website.

The Online Help S400 S600 integrated in the software (incl. ASCII Object Reference) can be started independently.

Comments

MOHAMED REDA's picture
MOHAMED REDA
how can i make set up for kollmorgen automation suite
i do not have the program
please i need your help
Will Gaffga's picture
Will Gaffga
The Kollmorgen Automation Suite (KAS IDE) is available for purchase through your local distributor. Unlike these other tools, it must be purchased.