Speed Sensor Programming Help
We are having trouble programming the AKD Basic drive to read a pulse from a speed sensor. We have a clutch coupled to motor and we want the motor to turn on when clutch reads a certain speed. The speed sensor is power by 24 VDC supply and the signal is connected to Digital input 1, pin 10 on X7 connector. The sensor is reading pulses from a gear tooth that has 36 teeth. The sensor has an operating frequency from 0 to 20 kHz. Rise fall time is <2 micro seconds. What would be the proper way to program the AKD to read the sensor?
Comments & Answers
Maybe I didn't understand...
Is the sensor's output signal
The sensor has a 0-5 vdc
The highest count frequency
I would suggest to count the pulses by the 2nd feedback input (FB2.SOURCE = 2, FB2.MODE=2, FB2.ENCRES = 36?) and read out the velocity by parameter <EXTENCODER.FREQ> in the program.
Thanks Joerg! We tried it
In reply to The highest count frequency by Joerg Muslewski
If you have the sensor wired