Back to top
File Description: 
KAS Runtime Firmware for PCMM. Note: PCMM Runtime version and KAS IDE version must be identical (e.g. both must have version 2.12.x.zzzz).
Language: 
English
Release: 
2.12
Release Date: 
Tuesday, February 6, 2018
File Description: 
KAS Runtime Firmware for PCMM. Note: PCMM Runtime version and KAS IDE version must be identical (e.g. both must have version 2.12.x.zzzz).
Language: 
English
Release: 
2.12
Release Date: 
Tuesday, February 6, 2018

Connecting to the PDMM

When connecting to a device for the first time, it is often confusing how to set up the initial communications.  Well, the PDMM and the IDE software for KAS make this task relatively simple.  There is nothing difficult about it once you know where to start.

1. Rotary Switch

Start with a pre-configured static IP address using the rotary switch (S1) positions 2 through 9.  These give IP addresses of 192.168.0.(100+S1).  So for switch position 3, the IP address is 192.168.0.103.

File Description: 
KAS Runtime Firmware for AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 2.12.x.zzzz).
Language: 
English
Release: 
2.12
Release Date: 
Tuesday, February 6, 2018
File Description: 
KAS Runtime Firmware for AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 2.12.x.zzzz).
Language: 
English
Release: 
2.12
Release Date: 
Tuesday, February 6, 2018
File Description: 
Provides overview, wiring diagram, electrical and mechanical specifications.
Language: 
English
Release: 
2.4
Release Date: 
Tuesday, October 31, 2017
File Description: 
Valid for KVB software 2.20 SP2 Build 2.22.353.0. This HMI program is set up to run motion tasks in the AKD drive. The operator can select from 5 motion tasks saved in the drive and run the selected task. The distance and speed of one other task can be edited by the operator. This program is also set up to run a manual jog move in velocity mode. For more information, see the application note included in this package.
Language: 
English
Release: 
2.20
Release Date: 
Monday, October 9, 2017
File Description: 
Valid for KVB software 2.20 SP2 Build 2.22.353.0. An HMI program that is setup to work with a Basic program in the AKD Basic drive. Allows the operator to select and execute five pre-programmed position moves saved in the Basic program. The operator can edit the distance and speed of one pre-programmed position move. Indicators show the status of motion. The HMI will indicate if homing is complete and the homing move can be started from the HMI.
Language: 
English
Release: 
2.20
Release Date: 
Monday, October 9, 2017

There are a number of KDN articles that contain videos, application notes, and demo programs to teach new users or refresh experienced users how certain features work. Below are links to these articles separated into sections based on the type of media they contain.

This video introduces the KAS IDE, ST (Structured Text) Editor

Covered in the Video:

  • Syntax
  • Compile, run, and animation
  • Comments
  • Using Function and Function Blocks
  • Conditional Statements
  • Shortcut keys
  • (Reference to) Debugging

Pages