Back to top

The AC Synchronous stepping motor may initially start in the opposite direction from the one desired.

The two conditions which determine the instantaneous starting direction of an AC Synchronous Stepping motor are the position of the rotor prior to start and what portion of the AC sine wave is apparent when it is first applied to the motor windings.

Curve A in the attached diagram shows the motor starting in the correct direction.