Back to top
File Description: 
Describes software installation, setup, and operation for the AKD PDMM drive. Includes basic topics and examples to help guide you in setting up and using the various features in the drive. Valid for KAS software version 2.12 and firmware version 1.16.
Language: 
English
Release: 
2.12
Release Date: 
Thursday, July 6, 2017

The KAS extended template shows the use of different basic functionality, when using the pipe network motion engine. It’s based on the standard two axis pipe network example and includes some of the most common use cases. It covers the following topics

  • PipeNetwork motion blocs (Master, Gear, Comparator, Cam, Phaser, Converter, Axis)
  • Programming languages (SFC, LD, ST)
  • Subprograms (Functions, UDFB)
  • Control Panel
  • Variable structures
  • Defines

Bezeichnungen der Stecker in den Kollmorgen Servoverstärkern.

The system covered includes a PxMM controller with up to twelve additional AKD drives.

All automation functions are handled in the PLC, the functionality covers the following:

File Description: 
Describes AKD PDMM Faults, warnings, error messages, and alarms. Provides cause and remedy instructions to help determine the specifics of the failure and to correct the underlying problem.
Language: 
Portuguese, Brazil
Release: 
1.15
Release Date: 
Monday, October 10, 2016
File Description: 
Describes AKD PDMM Faults, warnings, error messages, and alarms. Provides cause and remedy instructions to help determine the specifics of the failure and to correct the underlying problem.
Language: 
English
Release: 
1.15
Release Date: 
Monday, October 10, 2016
File Description: 
Describes AKD PDMM Faults, warnings, error messages, and alarms. Provides cause and remedy instructions to help determine the specifics of the failure and to correct the underlying problem.
Language: 
Chinese, Simplified
Release: 
1.15
Release Date: 
Monday, October 10, 2016
File Description: 
AKD PDMM Servo Drive (800 MHz) Firmware Motion Control EtherCAT. Note: This firmware complies with recently revised U.S. and E.U. export regulations (E.U. Dual Use Regulation 428/2009, and U.S. Dual-use regulation EAR Category 3 under ECCN3A225).
Language: 
English
Release: 
1.15
Release Date: 
Sunday, October 9, 2016
File Description: 
AKD PDMM Servo Drive (1.2 GHz) Firmware Motion Control EtherCAT. Note: This firmware complies with recently revised U.S. and E.U. export regulations (E.U. Dual Use Regulation 428/2009, and U.S. Dual-use regulation EAR Category 3 under ECCN3A225).
Language: 
English
Release: 
1.15
Release Date: 
Sunday, October 9, 2016

Hello sir,

Is AKD M01206-MCEC  suitable for application in which I want to rotate my motor at my required load torque with constant speed?

What are the Inputs & Outputs of the System?

Pages