Back to top

I'm using a 3rd Party HMI and if I use 32-bit-float to a REAL in the PDMM everything looks OK except I have a small difference because of rounding.

I would like to use integers but when I use 32-Bit-Signed on the HMI it dosen't match in the PDMM.

Example:   If I set my Numeric Format to 32 Bit Signed on the HMI and  in the Kollmorgen I set a DINT to 1.0 I see 16256 on the HMI.