Back to top

The DDL catalog shows a dynamic bend radius of 15X the cable diameter for the MxC, TxC, HxC cables.  The static bend radius for these cables would be 10X the cable diameter.  It is important note as stated in the DDL catalog, the cables exiting the motor and the hall assembly are not flex rated as well as the AKD interface cable ( either AKD-ACI-AKD-A or ACI-AKD-B connector interface adapter cables  ) and must be static in the application.