Back to top

Instructions for using the Hint3.exe program to load the bootloader and firmware into the S600

See the attached zip file for the Hint3.exe file and the bootloader file.

Place the Hint3.exe file in a folder on the C: drive.  Place the bootloader file (nb72_400) and firmware file (allxxx) in that same folder.

 

Downloading the bootloader file:

1.            Connect controller SR600 (S600 drive) with serial interface COM1.