Back to top

In some application low current brakes are used which may cause the drive to fault on F305 Brake Open Circuit.
Cause:
Motor brake open circuit. Fault threshold is 200 mA.
Remedy:
Check cabling and general functionality.

For special low current brake applications, the F305 fault can be bypassed

using the setting MOTOR.BRAKE = 100 set via the Workbench terminal.