Back to top

Attached are two subprograms that can be imported to the Project Explorer of the KAS IDE software. They are companions to the built in GetCtrlErrors function block which has a Q output that lets the user know if there is an active Alarm or Error, and will populate two boolean arrays of size 100 to let the user know which specific Alarms and Errors are currently active.