Back to top

The attachments outline a KAS Application with the following features:

  • 3 axis coordinated motion
  • Banner vision camera connected to the PDMM via Ethernet/IP
  • Camera reads a barcode and  sends the information through Ethernet/IP to the PDMM.
  • The bar code value is then used to determine which pattern to run

This article describes connecting a PDMM to a Cognex vision system via Ethernet/IP. It contains the following parts:

  • Application note
  • PDMM .kas project